R_LVDn_Create_UserInit

Performs user-defined initialization relating to the voltage detection circuit.

Remark This API function is called as the R_LVDn_Create callback routine.

[Syntax]

void R_LVDn_Create_UserInit ( void );

Remark n is the circuit number.

[Argument(s)]

None.

[Return value]

None.