r_rspin_receive_interrupt

Performs processing in response to the receive buffer full interrupts.

Remark This API function is called to run interrupt processing for the receive buffer full interrupt.

[Syntax]

static void r_rspin_receive_interrupt ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.