r_s12adn_interrupt

Performs processing in response to the A/D scan end interrupt.

Remark This API function is called to run interrupt processing for the A/D scan end interrupt, which is generated on completion of scanning of the analog inputs.

[Syntax]

static void r_s12adn_interrupt ( void );

Remark n is the unit number.

[Argument(s)]

None.

[Return value]

None.