r_scin_callback_transmitend

Performs processing in response to the transmit-end interrupts.

Remark This API function is called as the r_scin_transmitend_interrupt callback routine.

[Syntax]

static void r_scin_callback_transmitend ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.