[RI78V4] tab

Outline

This tab shows the detailed information on the RI78V4 to be used categorized by the following.

- Version Information

Display image



Explanation of each area

1 ) [Version Information]

The detailed information on the version of the RI78V4 are displayed.

Kernel version

Display the version of the RI78V4 to be used.

Note that the version is set permanently when the project is created, and cannot be changed.

Default

Using the RI78V4 version

How to change

Changes not allowed

Install folder

Display the folder in which the RI78V4 to be used is installed with the absolute path.

Default

The folder in which the RI78V4 to be used is installed

How to change

Changes not allowed

Memory model

Display the memory model set in the project.

Display the same value as the value of the [Memory model type] property of the build tool.

Default

The memory model selected in the property of the build tool

How to change

Changes not allowed