-
loc_cpu
iloc_cpu
-
ER loc_cpu ( void );
ER iloc_cpu ( void );
|
CALL !!_loc_cpu
CALL !!_iloc_cpu
|
These service calls change the system status type to the CPU locked state.
As a result, maskable interrupt acknowledgment processing is prohibited during the interval from this service call is issued until
unl_cpu or
iunl_cpu is issued, and service call issuance is also restricted.
If a maskable interrupt is created during the interval from this service call is issued until
unl_cpu or
iunl_cpu is issued, the RI78V4 delays transition to the relevant interrupt processing (interrupt handler) until either
unl_cpu or
iunl_cpu is issued.
The service calls that can be issued in the CPU locked state are limited to the one listed below.
|
|
|
|
|
|
|
|
|
|
|
Reference dispatching state.
|
|
Reference dispatch pending state.
|
Note 1 The CPU locked state changed by issuing this service call must be cancelled before the processing program that issued this service call ends.
Note 2 This service call does not perform queuing of lock requests. If the system is in the CPU locked state, therefore, no processing is performed but it is not handled as an error.
Note 3 The RI78V4 implements disabling of maskable interrupt acknowledgment bu manipulating the interrupt mask flag register (MK
xx) and the in-service priority flag (ISP
x) of the program status word (PSW). Therefore, manipulating of these registers from the processing program is prohibited from when this service call is issued until
unl_cpu or
iunl_cpu is issued.