twai_sem

Outline

Acquire semaphore resource (with timeout).

C format

 ER      twai_sem ( ID semid, TMO tmout );


Assembly format

 MOVW    BC, #tmout_lo
 MOVW    DE, #tmout_hi
 MOV     A,  #semid
 CALL    !!_twai_sem


Parameter(s)

I/O

Parameter

Description

I

 ID      semid;
ID number of the semaphore from which resource is acquired.

I

 TMO     tmout;
Specified timeout (unit: ticks).

TMO_FEVR: Waiting forever.

TMO_POL: Polling.

Value: Specified timeout.



Explanation

This service call acquires a resource from the semaphore specified by parameter semid (subtracts 0x1 from the semaphore counter).

If a resource could not be acquired from the target semaphore (semaphore counter is set to 0x0) when this service call is issued, the counter manipulation processing is not performed but the invoking task is queued to the target semaphore wait queue in the order of resource acquisition request (FIFO order).

As a result, the invoking task is unlinked from the ready queue and is moved from the RUNNING state to the WAITING state (waiting state for a semaphore resource).

Waiting State for a Semaphore Resource Cancel Operation

Return Value

The resource was returned to the target semaphore as a result of issuing sig_sem.

E_OK

The resource was returned to the target semaphore as a result of issuing isig_sem.

E_OK

Forced release from waiting (accept rel_wai while waiting).

E_RLWAI

Forced release from waiting (accept irel_wai while waiting).

E_RLWAI

Polling failure or timeout.

E_TMOUT



Note When TMO_FEVR is specified for wait time tmout, processing equivalent to wai_sem will be executed. When TMO_POL is specified, processing equivalent to pol_sem will be executed.

Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_RLWAI

-49

Forced release from waiting (accept rel_wai/irel_wai while waiting).

E_TMOUT

-50

Polling failure or timeout.