17.5.5 Mailbox information
The number of items that can be defined as mailbox information is limited to one for each ID number.
The following shows the mailbox information format.
CRE_MBX (mbxid, { mbxatr, maxmpri, mprihd });
|
The items constituting the mailbox information are as follows.
Specifies the ID number for a mailbox.
A value from 0x1 to 0xff, or a name, can be specified for
mbxid.
Note When a name is specified, the CF850V4 automatically assigns an ID number.
The CF850V4 outputs the relationship between a name and an ID number to the system information header file in the following format:
#define mbxid value
Specifies the attribute for a mailbox.
The keyword that can be specified for
mbxatr is TA_TFIFO, TA_TPRI, TA_MFIFO and TA_MPRI.
TA_TFIFO: Task wait queue is in FIFO order.
TA_TPRI: Task wait queue is in task priority order.
TA_MFIFO: Message wait queue is in FIFO order.
TA_MPRI: Message wait queue is in message priority order.
3 ) Maximum message priority:
maxmpri
Specifies the maximum message priority for a mailbox.
A value from 0x1 to 0x7fff can be specified for
maxmpri.
Note maxmpri is valid only when TA_MPRI is specified for mqueue.
It is invalid when TA_MFIFO is specified for mqueue.
4 ) Reserved for future use:
mprihd
System-reserved area.
Values that can be specified for
mprihd are limited to NULL characters.