17.4 System Information
The following describes the format that must be observed when describing the system information in the system configuration file.
The GOTHIC-FONT characters in following descriptions are the reserved words, and italic face characters are the portion that the user must write the relevant numeric value, symbol name, or keyword.
Items enclosed by square brackets "[ ]" can be omitted.
17.4.1 RI series information
Only one information item can be defined as RI series information.
The following shows the RI series information format.
RI_SERIES (rtos_name, rtos_ver);
|
The items constituting the RI series information are as follows.
1 ) Real-time OS name:
rtos_name
Specifies the real-time OS name.
The keyword that can be specified for
rtos_name is the RI850V4.
2 ) Version number:
rtos_ver
Specifies the version number for the RI850V4.
In RI_SERIES, values specifiable for
rtos_ver is the "V2xy"(as version number).
Note
If the version number of RI850V4 is "V2.01.23", rtos_ver should be set to "V201".