-h


This option displays the descriptions of ccrh options.

[Specification format]

-h

 

-

Interpretation when omitted

The descriptions of ccrh options are not displayed.

[Detailed description]

-

This option outputs the descriptions of ccrh options to the standard error output.
It does not execute compilation.

[Example of use]

-

To output the descriptions of ccrh options to the standard error output, describe as:

>ccrh -h -Xcommon=rh850