This option specifies that an object for the specified core is generated.
[Specification format]
- | Interpretation when omitted |
An object for G3M is generated.
[Detailed description]
- | This option specifies that an object for core core is generated. |
- | The items that can be specified as core are shown below. |
|
g3m
|
Generates an object for G3M.
|
|
g3k
|
Generates an object for G3K.
|
|
g3mh
|
Generates an object for G3MH. [V1.02.00 or later]
|
|
g3kh
|
Generates an object for G3KH. [V1.03.00 or later]
|
|
g4mh
|
Generates an object for G4MH. [V2.00.00 or later]
|
- | If this option is specified more than once, the last specification is valid. |
- | An error will occur in any of the following cases. |
- | When the parameter is omitted |
- | When a parameter that is not specifiable is specified |