-Xmulti_level


This option specifies the generation of a multi-core program.

[Specification format]

-Xmulti_level=level

 

-

Interpretation when omitted

A single-core program is generated.

[Detailed description]

-

This option generates a program for the specified core.

-

The items that can be specified as level are shown below.
An error will occur if any other item is specified.

0

Generates a single-core program.

The #pragma pmodule directives in the program are ignored.

1

Generates a multi-core program.

The #pragma pmodule directives in the program become valid.

[Example of use]

-

To generate a multi-core program, describe as:

>ccrh -Xmulti_level=1 -Xcommon=rh850 file1.c file2.c