-Xasm_option


This option specifies assemble options.

[Specification format]

-Xasm_option=arg

 

-

Interpretation when omitted

The ccrh driver interprets all specified options.

[Detailed description]

-

This option passes arg to the assembler as the assemble option.

-

An error will occur if arg is a non-existent assemble option.

-

An error will occur if arg is omitted.

[Example of use]

-

To pass the -Xprn_path option to the assembler, describe as:

>ccrh -Xasm_option=-Xprn_path -Xcommon=rh850 main.c

 

The example above has the same meaning as the following.

>ccrh -S -Xcommon=rh850 main.c
>asrh -Xprn_path -Xcommon=rh850 main.asm