-Xcommon


This option specifies that an object file common to the various devices is generated.

[Specification format]

-Xcommon=series

 

-

Interpretation when omitted

None

[Detailed description]

-

This option specifies that an object file common to the various devices is generated.

-

This option is invalid in V2.00.00 or later versions. If this option is specified, it will be ignored but no error will occur due to the compatibility with conventional versions. No warning is output in this case.

-

v850e3v5 or rh850 can be specified for series.

-

An error will occur in any of the following cases.

-

When series is omitted

-

When a parameter that is not specifiable is specified for series

-

When this option is omitted [V1.01.00 or earlier]

[Remark]

This option does not affect the output code.

When selecting the instruction set to be used, specify the -Xcpu option.