-U


This option deletes the assembler symbol definition by the -D option.

[Specification format]

-Uname[,name]...

 

-

Interpretation when omitted

None

[Detailed description]

-

This option deletes the definition of assembler symbol name by the -D option.

-

An error will occur if name is omitted.

-

This option cannot delete the definition by describing "name .SET def".

-

This option can be specified more than once.

-

If both this option and -D option are specified for the same assembler symbol, the option specified last will be valid.

[Example of use]

-

To delete the definition of assembler symbol "test" by the -D option, describe as:

>asrh -Utest -Xcommon=rh850 main.asm