-FIX_RECORD_LENGTH_AND_ALIGN [V1.07.00 or later]


Fixes the format of data records to be output.

[Specification format]

-FIX_RECORD_LENGTH_AND_ALIGN=align

 

-

Interpretation when omitted

None

[Detailed description]

-

This option is used to output an Intel HEX file or a Motorola S-record file with records of a fixed length starting from the address that has alignment with the specified number.

-

The address of the first record to be output should be less than or equal to the first address of a section and be the largest number that can be divided by the specified alignment number.

-

The specified numerical value or default value for the parameter of the -BYte_count option will be used as the length of the records.

-

Since the length of records is fixed, each record may include data for more than one section.

-

In unused areas, the value specified by the -SPace option will be output. If the -SPace option is not specified, 0 (with the -CRC option not specified) or 0xFF (with the -CRc option specified) as the default value will be output.

[Example of use]

-

Starting the output of records from an address that can be divided by 8, with the length of each record fixed to 16 bytes (10 in hexadecimal)

>rlink a.obj b.obj -form=hexadecimal -byte_count=10 -fix_record_length_and_align=8

[Remark]

-

If the -form={hexadecimal|stype} option is not specified, this option will be invalid.