This option checks the consistency of the address to which the section is allocated.
This option checks the consistency of the address to which the section is allocated. |
The items that can be specified as type are shown below. |
Allocates the section to a fixed-address area (e.g. I/O area). If the address range overlaps with ROM or RAM, the setting for FIX is valid. |
Specify the start address and end address of the address range to check for consistency in hexadecimal as address1 and address2. |
The result is normal when section .text and section .bss are respectively allocated within the ranges from 0x100 to 0x1FF and from 0x200 to 0x2FF. |
If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid. |