Renesas Electronics
The character string of the command line of the assembler is output.
The output example of the command line information is shown below.
Command Line Parameter
a.asm -Xcommon=rh850 -Xprn_path (1)
Number
Description
(1)
Character string of command line
The character string of the command line specified for the assembler is output.