Renesas Electronics
Messages for errors or warnings are output.
The output example of the error information is shown below.
*** Error Information ***
** E0561200 Backed up file "sample1.lib" into "usrlib.lbk" (1)
Number
Description
(1)
Message
The message is output.