Renesas Electronics
This section explains the implementation-defined behavior of the CC-RH which is compliant with the C90 and C99 standards.
See "4.2 Extended Language Specifications" for extended language specifications explicitly added by the CC-RH.