The term value 2 complement is sought.
[Function]
Returns the value of the term of an expression by the two's complement.
[Application example]
(1) | -1 becomes the two's complement of 1.
0000 0000 0000 0000 0000 0000 0000 0001 becomes:
1111 1111 1111 1111 1111 1111 1111 1111
Therefore, with the .set directive, the value "0xFFFFFFFF" is defined in the symbol "NO". |