!


Obtains the logical negation by each bit.

[Function]

Negates the value of the term of an expression on a bit-by-bit basis and returns the result.

[Application example]

mov     !0x3, r10       ; (1)

(1)

Logical negation is performed on "0x3" as follows:
0xFFFFFFFC is returned.