5.1.6 Shift operators

The following shift operators are available.

Operator

Overview

>>

Obtains only the right-shifted value of the first term which appears in the second term.

<<

Obtains only the left-shifted value of the first term which appears in the second term.