Specifies an offset from the first address of a section.
The .offset directive specifies an offset from the first address of a section that holds instruction code for the lines following the .offset directive.  | 
If .offset is written prior to any section definition directive at the beginning of a source program, the name of the section will be ".text" and the relocation attribute will be "TEXT".  | 
The operand value is in accordance with "Absolute expression". An illegal value will lead to an error and cause processing to end.  | 
The overall definition of a single section may contain multiple .org directives. Note, however, that an error occurs when the specified value is smaller than that for a preceding .offset directive.  | 
The value specified as an operand of the .offset directive must be an Absolute expression in the range of 0x0 to 0x7fffffff.  | 
The initial value for the area that is formed between the location of the .offset directive and the specified offset is 0x0.  | 
When the .offset directive is written in a section with relocation attribute "BSS", an error will occur.  |