Indicates the end of the control range of a conditional assembly control instruction.
With these conditional assembly control instructions, source statements subject to assembly can be changed without major modifications to the source program.  | 
If a statement for debugging that becomes necessary only during the program development is described in a source program, whether or not the debugging statement should be assembled (translated into machine language) can be specified by setting switches for conditional assembly.  |