This section describes the output formats of messages.
The output formats of messages are as follows.
(1)  | When the file name and line number are included  | 
 
file-name (line-number) : message-type 05 message-number : message 
 | 
 
(2)  | When the file name and line number aren't included  | 
 
message-type 05 message-number : message 
 | 
 
Remark  | Following contents are output as the continued character string.  | 
 
Message Types														:	1 alphabetic character
Messages														:	5 digits