&


Obtains the logical AND operation for each bit of the first and second term values.

[Function]

Performs an AND (logical product) operation between the value of the 1st term of an expression and the value of its 2nd term on a bit-by-bit basis and returns the result.

[Application example]

MOV     A, #0x6FA & 0x0F        ; (1)

(1)

AND operation is performed between the two values "0x6FA" and "0x0F" as follows:
This operation loads "0xF0A" in the A register.