[Extended Service Call Routine] tab

This tab displays the extended service call routine information (e.g. Function Code and Start Address) of the RI850V4.

Figure A-26. [Extended Service Call Routine] Tab



The following items are explained here.

- [How to open]

- [Description of each area]

- [Context menu]

[How to open]

- From the [Debug] menu, select [Download].

- From the [View] menu, select [Realtime OS] >> [Resource Information].

[Description of each area]

(1) Information display area

This area displays the extended service call routine information (e.g. Function Code and Start Address) of the RI850V4.

This area consists of the following items.

Function Code

The function code of the extended service call routine is shown.

Start Address

The start address of the extended service call routine is shown.

Attribute

The coding language of the extended service call routine is shown.

TA_HLNG

C language

TA_ASM

Assembly language



Remark Double-clicking an extended service call routine information cell (such as Function Code or Start Address) displays the source file of the extended service call routine in the Editor panel and moves the caret to the relevant location.

[Context menu]

The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.

(1) Header row

Display

Displays cascade menus for selecting the header items to display.

Selected item name

The following items are displayed for selection.

Function Code, Start Address, Attribute

Checked

The item in question will be displayed.

Not checked

The item in question will not be displayed.

Notation

Displays cascade menus for selecting the display notation.

Selected item name

The following items are displayed for selection.

Function Code, Start Address

DEC

Displays value in signed decimal number.

HEX

Displays value in hexadecimal number.



(2) Footer row

Jump to Source (Start Address)

Opens the Editor panel, and displays the source code of the extended service call routine.

Jump to Disassemble (Start Address)

Opens the Disassemble panel, and displays the results of disassembling the extended service call routine.

Reset Display Item

Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).