2.2.1.1 [Full-spec emulator]

Connect a host machine and Full-spec emulator. If required, connect a target board, too.

For details on the connection method, see the user's manual for Full-spec emulator.

Figure 2.1

Connection Example [Full-spec emulator]