2.13.4 Collect execution history only when the condition is met

The program execution history can be collected only when a condition is met.

By setting a Point Trace event, the execution history is collected as trace data only when an arbitrary variable or I/O register is accessed with the specified type.

To use this function, follow the procedure described below.

 

2.13.4.1 Set a Point Trace event

2.13.4.2 Execute the program

2.13.4.3 Edit a Point Trace event [Full-spec emulator][E1][E20]

2.13.4.4 Delete a Point Trace event