2.13.6.2  
Change display format of values
 
The display format of the [Line Number/Address], [Address] and [Data] area can be changed using buttons below on the toolbar. 
Note that these buttons are disabled while the tracer is running.
| 
 
Notation 
 | 
 
The following buttons to change the notation of a data value are displayed.  
 | 
| 
 
  
 | 
 
 
Hexadecimal 
 | 
 
Displays values on this panel in hexadecimal number (default). 
 | 
| 
 
 
Decimal 
 | 
 
Displays values on this panel in decimal number. 
 | 
| 
 
 
Octal 
 | 
 
Displays values on this panel in octal number. 
 | 
| 
 
 
Binary 
 | 
 
Displays values on this panel in binary number. 
 |