The LPD clock is used for time measurement by a Run-Break Timer event (see "2.14.1 Measure execution time until stop of the execution" for details) or a Timer Result event (see "2.14.2 Measure execution time in a section" for details). The measurable time is as follows:
The CPU clock is used for time measurement by a Run-Break Timer event (see "2.14.1 Measure execution time until stop of the execution" for details) or a Timer Result event (see "2.14.2 Measure execution time in a section" for details).