In the program execution process, the performance in a section can be measured by setting a Performance Measurement event.
To use this function, follow the procedure described below.
2.15.1.1 Set a Performance Measurement event
2.15.1.3 Edit a Performance Measurement event
2.15.1.4 Delete a Performance Measurement event
Also see "2.18.6 Notes for setting events" for details on Performance Measurement events (e.g. limits on the number of enabled events). |