2.6.3 Run a build in parallel with other operations

CS+ can automatically start a build when one of the following events occurs (rapid build function).

 

-

For other than the debug-only project

-

When any one of the following files that are added to the project is updated:
(C source file, assembly source file, header file, link directive file, symbol information file, object module file, or library file)

-

When a build target file has been added to or removed from the project

-

When the link order of object module files and library files is changed

-

When the property of the build tool or the build target file is changed

-

For the debug-only project

-

When you have edited and saved the C source file, assembly source file and header file that are added to the debug-dedicated project

-

When a C source file, assembly source file, or header file has been added to or removed from the debug-dedicated project

-

When the property of the debug-dedicated project is changed

 

If a rapid build is enabled, it is possible to perform a build in parallel with the above operations.

To enable/disable a rapid build, select [Rapid Build] from the [Build] menu. A rapid build is enabled by default.

Caution

When an external text editor is used, check the [Observe registered files changing] check box on the [General - Build/Debug] category in the Option dialog box to enable this function.

Remark 1.

After editing source files, it is recommend to save frequently by pressing the [Ctrl] + [S] key.

Remark 2.

Enable/Disable setting of the rapid build applies to the entire project (main project and subprojects).

Remark 3.

If you disable a rapid build while it is running, it will be stopped at that time.