The program in execution is forcibly stopped by clicking the 
 button on the debug toolbar (Forced break function). 
In cases of failure to stop a program during execution, the following setting may be required to allow stopping execution of the program.  | 
The [Reset While Running] category on the [Debug Tool Settings] tab of the Property panel  |