2.11.3.1
Search for an I/O register
An I/O register can be searched for.
Specify the I/O register name to search with the text box in the search area (case-insensitive). You can either type character strings directly from the key board (up to 512 characters), or select one from the input history via the drop-down list (up to 10 items). Then, click either one of the following button.
|
Searches up for the I/O register name containing the string specified in the text box, and selects the I/O register that is found.
|
|
Searches down for the I/O register name containing the string specified in the text box, and selects the I/O register that is found.
|
Remark 1. | The hidden I/O register name being classified with a category can be searched (the category is opened and the I/O register is selected). |
Remark 2. | After typing character strings to search, to press the [Enter] key is the same function as clicking the
button, and to press the [Shift] + [Enter] key is the same function as clicking the
button. |