[Hook Transaction Settings] tab


This tab is used to display the detailed information categorized by the following and the configuration can be changed.

For details on the hook transaction, see "2.16 Use Hook Function".

 

(1) [Hook Transaction Settings]

[Description of each category]

(1)

[Hook Transaction Settings]

The detailed information on the hook transaction is displayed and its configuration can be changed.

Note that the properties on this tab can be specified via the Text Edit dialog box, which is opened by clicking the [...] button that appears at right edge of a field when you select each property (you cannot specify the process directly on this panel).

Caution

Up to 64 characters for one process, and up to 128 processes for each property can be set (one line in the [Text] area in the Text Edit dialog box is equivalent to one processing).

Before download

Specify the process to proceed right before downloading the load module file.

Default

Before download[0] ("[]" is the current number of specified processes.)

Modifying

Specify with the Text Edit dialog box.

Format

Either one of the following

-

SFR name + space + Value

[Process] Automatically overwrites the value of SFR with Value.

-

CPU register name + space + Value

[Process] Automatically overwrites the value of CPU register with Value.

-

Source + space + Python script path

[Process] Automatically executes a script file specified with Python script path.

After download

Specify the process to proceed right after downloading the load module file.

Default

After download[0] ("[]" is the current number of specified processes.)

Modifying

Specify with the Text Edit dialog box.

Format

Either one of the following

-

SFR name + space + Value

[Process] Automatically overwrites the value of SFR with Value.

-

CPU register name + space + Value

[Process] Automatically overwrites the value of CPU register with Value.

-

Source + space + Python script path

[Process] Automatically executes a script file specified with Python script path.

After CPU reset under breaking

Specify the process to proceed right after CPU reset during break.

Default

After CPU reset under breaking[0] ("[]" is the current number of specified processes.)

Modifying

Specify with the Text Edit dialog box.

Format

Either one of the following

-

SFR name + space + Value

[Process] Automatically overwrites the value of SFR with Value.

-

CPU register name + space + Value

[Process] Automatically overwrites the value of CPU register with Value.

-

Source + space + Python script path

[Process] Automatically executes a script file specified with Python script path.

Before running

Specify the process to proceed right before the execution of the program.

Default

Before running[0] ("[]" is the current number of specified processes.)

Modifying

Specify with the Text Edit dialog box.

Format

Either one of the following

-

SFR name + space + Value

[Process] Automatically overwrites the value of SFR with Value.

-

CPU register name + space + Value

[Process] Automatically overwrites the value of CPU register with Value.

-

Source + space + Python script path

[Process] Automatically executes a script file specified with Python script path.

After breaking

Specify the process to proceed right after the program break.

Default

After breaking[0] ("[]" is the current number of specified processes.)

Modifying

Specify with the Text Edit dialog box.

Format

Either one of the following

-

SFR name + space + Value

[Process] Automatically overwrites the value of SFR with Value.

-

CPU register name + space + Value

[Process] Automatically overwrites the value of CPU register with Value.

-

Source + space + Python script path

[Process] Automatically executes a script file specified with Python script path.