2.2.1.3 [E20]

Connect a host machine and E20. If required, connect a target board, too.

See E20 User's Manual for details on the connection method.

Figure 2.3

Connection Example [E20]

Caution

Only serial communications are supported as the communication method with the target board (JTAG communications is not available).