2.11.7
Clear the trace memory
To clear the collected trace data contents, click the
button on the toolbar.
Note that this button is disabled while a tracer is running.
Remark 1. | [IECUBE][Simulator]
When [Yes] is specified in the [Clear trace memory before running] property in the [Trace] category on the [Debug Tool Settings] tab of the Property panel, the trace memory is cleared each time a program is executed. |
Remark 2. | [E1][E20][EZ Emulator]
The trace memory is cleared each time a program is executed (fixed). |