2.9.6.2 Organize the registered watch-expressions

Registered watch-expressions can be organized in categories (folders) and displayed in tree view (there is no category as default).

Caution 1.

Categories cannot be created within categories.

Caution 2.

Up to 64 categories can be created in one watch panel (if this restriction is violated, a message appears).

(1)

Create new category

Move the caret to the position to create a new category then click the button in the toolbar and directly enter the new category name.

(2)

Edit category name

Click the category name to edit, and click it again, then directly modify the category name from the keyboard.

(3)

Delete categories

Select categories to delete then click the button in the toolbar.

(4)

Change the display order

Registered watch-expressions are categorized when they are dragged and dropped in the category.

Also, the display order of the categories and the watch-expressions (upper or lower position) can be changed easily by drag and drop operation.

Remark

Drag and drop the watch-expressions/categories in other watch panel (Watch1 to Watch4) to copy them.