2.5.2 Advanced downloading

You can change the download files and the condition to download.

With CS+, the following file types can be downloaded.

Table 2.1

Downloadable File Formats

Downloadable File

Extension

File Format

Load module file

.abs

Load module format

Intel Hex file

.hex

Intel Hex file format

Motorola S-record file

.mot

Motorola S-record file format

-

(S0, S1, S9 - 16 bit-address)

-

(S0, S2, S8 - 24 bit-address)

-

(S0, S3, S7 - 32 bit-address)

Binary file

.bin

Binary format

 

You can change the download files or download conditions in the following Download Files dialog box.

The Download Files dialog box is opened by clicking the [...] button that appears at the right edge in the column of the [Download files] property when you select it in the [Download] category on the [Download File Settings] tab of the Property panel.

Figure 2.68

Opening Download Files Dialog Box

Figure 2.69

Advanced Downloading (Download Files Dialog Box)

 

This section describes how to configure on the Download Files dialog box above when the following cases.

For details on the contents and function in each area, see the section for the Download Files dialog box.

 

2.5.2.1 Change download conditions for load module files

2.5.2.2 Add download files (*.hex/*.mot/*.bin)

2.5.2.3 Perform source level debugging with files other than the load module file format