Renesas Electronics
top
Debug Tool
FUNCTIONS
Preparation before Debugging
2.2 Preparation before Debugging
This section describes the preparation to start debugging the created program.
Differences Information
Previous Topic
Overview
Next Topic
Confirm the connection to a host machine
Table of Contents
Overview
Preparation before Debugging
Confirm the connection to a host machine
Configuration of Operating Environment of the Debug Tool
Connect to/Disconnect from the Debug Tool
Download and Upload
Displaying and Changing Programs
Usage of PIC/PID Function
Setting Overlay Sections
Execute Programs
Stop Programs (Break)
Displaying and Changing Memory, Registers, and Variables
Display Function Call Information from the Stack
Collecting an Execution History
Measuring the Execution Time
Measure Coverage [Simulator] [E20 [RX71M, RX66x, RX65x, and RX64M Groups]]
Set an Action into Programs
Event Management
Setting Up the Hook Process
Measuring Current Consumption [E2]
Using the Debug Console
About Input Value
Differences between the Microcontroller and the Emulator
Other Notes on Usage [E1] [E20] [EZ Emulator]