2.10.2 Stop the program at the arbitrary position (breakpoint)

The program in execution can be stopped at the arbitrary position by setting a breakpoint. A breakpoint can be set with a single click of the mouse.

You need to configure the type of breakpoints to use before setting a breakpoint.

This section describes the following.

 

2.10.2.1 Set the type of breakpoints/break timing to use [E1] [E20] [EZ Emulator]

2.10.2.2 Set a breakpoint

2.10.2.3 Edit a hardware breakpoint

2.10.2.4 Delete a breakpoint

 

Caution

[E1/E20/EZ Emulator [RX630, RX631, RX63N, RX63T, RX210, RX110, RX111 and RX113 Groups]]
If a break is generated by an execution-related break that is set to the WAIT instruction or an instruction immediately preceding it, an error may occur. To cause the target program to break at the WAIT instruction or an instruction immediately preceding it, use a breakpoint.