2.12.1.3 Displaying local variables

Selecting [Jump to Local Variable at This Time] from the context menu will open the Local Variables panel which displays local variables of the function indicated by the selected line.