This chapter describes the message types displayed by CS+.
 
The message types (1 alphabetic character) when CS+ is operated are as follows.
| 
 | 
 | 
| 
 | 
 
Internal error 
 | 
 
Processing terminated (suspended) due to internal error. 
 | 
| 
 | 
 
Fatal error 
 | 
 
Processing terminated (suspended) due to fatal error. 
 | 
| 
 | 
 
Information 
 | 
 
Informational message.  Check the message and continue the process. 
 | 
| 
 | 
 
Choice 
 | 
 
This type of message is displayed when a choice is necessary in order to carry on with the next operation.  It performs the selected action. 
 | 
| 
 | 
 
Warning 
 | 
 
Warning message.  Check the message and continue the process. 
 |