B.3.9 CS+ Python property (for build tool)
Below is a list of CS+ Python properties (for the build tool).
Table B.9 | CS+ Python Property (For Build Tool) |
|
|
build.Compile.AdditionalOptions
|
This property sets or refers to the compile options for the active project regarding other additional options.
|
build.Compile.IncludePath
|
This property sets or refers to the compile options for the active project regarding additional include paths.
|
build.Compile.Macro
|
This property sets or refers to the compile options for the active project regarding defined macros.
|
build.IsBuilding
|
This property confirms whether a build is running.
|
build.Link.AdditionalOptions
|
This property sets or refers to the link options for the active project regarding other additional options.
|
build.Link.LibraryFile
|
This property sets or refers to library files of the active project.
|
build.Link.SectionAlignment
|
This property sets or refers to the link options for the active project regarding section alignment.
|
build.Link.SectionROMtoRAM
|
This property sets or refers to the link options for the active project regarding sections where symbols are mapped from ROM to RAM.
|
build.Link.SectionStartAddress
|
This property sets or refers to the link options for the active project regarding the addresses where sections start.
|
build.Link.SectionSymbolFile
|
This property sets or refers to the link options for the active project regarding sections whose external defined symbols are to be output to a file.
|
build.ROMization.OutputObjectFile
|
This property sets or refers to the setting for output of a ROMized object file, that is, the value of the ROMization process option for the active project.
|
build.Version
|
This property refers to the version of the compiler package.
|