4. Downloading a load module file to E1.
In this step, you download the load module file generated by the build process to the target.
When the download is complete, you can run the program.
Click the Download button in the menu. |
The status bar of the Main Window changes as shown below. |