Running and Stopping the Program

2. Stopping the program

In this step, you stop the program.

Click the Stop button.

This stops the program and displays [BREAK] in the status bar.

The source code line where the program stopped or the current position of the program counter (PC) is highlighted in yellow.