This section describes an overview of the sample program and RH850/F1L(176pin) board.
1. Overview of the Program
The program is simple program which causes LEDs flash alternately.
![]() |
LEDs flash alternately
2. Overview of RH850/F1L(176pin) board
The following is an overview of RH850/F1L(176pin) board.
Evaluation LED1-4 : Lights in yellow when the P8_4 to P8_7 is LOW.
14pin connector : Used for on-chip debugging and writing.