2. Load the sample project
In this step, load the sample project.
In the "Load Sample Project" field, from the "RX" tab, select " RH850_F1L_Tutorial_Basic_Operation ", then click [GO]. |
Follow the on-screen instructions. A sample program opens as shown in the figure below. |